Part Number: AM2432
Tool/software:
Hi,
I have two problems with SNMP in Profinet.
I am using the SDK 09.02.15 with AM2432.
The first one is that I noticed that in the file pn_app_iod_cfg.h it is possible to modify macros that change the behavior of SNMP. I have tried to modify some values (such as PN_API_IOD_SNMP_PORT1_NAME and PN_API_IOD_SNMP_INTERFACE_NAME) but when querying the device with an external tool it seems that the values are fixed constants and those macros are not actually used. Is this normal behavior?
The second is that our team has performed a cybersecurity scan with the tool Nessus, and the two problems in the screen were found. Is it possible to take action on my side to be able to fix them? Or are these problems only fixable by correcting them in the stack?

Thanks.
Kind regards,
Andrea