Part Number: MSPM0C1104
Tool/software:
I create some PWM examples from CCS, and then 'Build Project' and 'Debug Project'
Before I flash MCU FW to USB4 MB, I can run examples normally with debug mode.
(The connected way (PWM:PA23, ATTACH: PA2, SENSOR: PA24) is the same as the following image)

After flashing MCU FW to USB4 MB, I got a such error....

How do I fix it and run examples normally with USB4 MB+Fan ?