Part Number: AM2634
Tool/software:
Do we support an Ethernet packet payload of less than 46 bytes?
Eg if a packet with a 4 byte payload was transferred how would it be handled by the AM2634?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2634
Tool/software:
Do we support an Ethernet packet payload of less than 46 bytes?
Eg if a packet with a 4 byte payload was transferred how would it be handled by the AM2634?
Thanks
Hi Chris,
As per IEEE Standard, the minimum ethernet frame size is 64B, out of which 18B are fixed for packet headers (Source and destination MAC addresses, FCS, Length). If you want to send a smaller packet than 64B, it will be an invalid packet format.
Instead you like be adding padding to increase length of the packet and meeting minimum packet size. This packet will then be processed by the AM26x device.
Regards,
Shaunak