Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hey there,
I adapted the example project mcan_message_rx_LP_MSPM0G3507_nortos_ticlang for receiving of CAN message.
If I send a CAN message from my PC CAN dongle (PCAN VIEW) the MSPM0G3507 triggers a CAN-RX-Interrupt and receives and processes the received message.
From time to time a single message does not trigger and interrupt..
But when I send a second message before the first one is processed, the second one is not processed.
And when I send multiple messages in a short time the CAN reveive seems to get completely stuck. Even if I wait some time a new CAN message won't trigger a new interrupt.
I need to restart my debug session to be able to receive CAN messages again.
I made a "watch expression" on "gInterruptLine1Status".
It changes to 0x0002000C or 0x00020004 when the receiving stops.
From the technical reference manual I found out that this seems to be the (raw or masked) interrupt status register value. And the SEC (single error correction) and/or the DED (dual error detection) bits are set.
I added/edited the following configurations to my sysconfig to somehow trigger an interrupt or anything else to be able to deal with the "getting stuck".
MCAN1.m0interrupts = ["DL_MCAN_MSP_INTERRUPT_DOUBLE_ERROR_DETECTION","DL_MCAN_MSP_INTERRUPT_LINE0","DL_MCAN_MSP_INTERRUPT_LINE1","DL_MCAN_MSP_INTERRUPT_SINGLE_ERROR_CORRECTION "]; MCAN1.interruptLine = ["DL_MCAN_INTR_LINE_NUM_0","DL_MCAN_INTR_LINE_NUM_1"]; MCAN1.rxFIFO0size = 10; MCAN1.rxFIFO0waterMark = 8; MCAN1.interruptFlags = ["DL_MCAN_INTERRUPT_RF0F","DL_MCAN_INTERRUPT_RF0N","DL_MCAN_INTERRUPT_RF0W"]; MCAN1.interruptLine0Flag = ["DL_MCAN_INTERRUPT_RF0F","DL_MCAN_INTERRUPT_RF0W"];
But none of my interrupt cases get triggered apart from the rx interrupt. This is my CAN-interrupt-handler:
void MCAN0_INST_IRQHandler(void)
{
printf("\nCAN_IRQ_handler");
switch (DL_MCAN_getPendingInterrupt(MCAN0_INST)) {
case DL_MCAN_IIDX_LINE0: // RX FIFO 0 Full - interrupt
__BKPT(0);
/* Check MCAN interrupts fired during TX/RX of CAN package */
gInterruptLine0Status |= DL_MCAN_getIntrStatus(MCAN0_INST);
DL_MCAN_clearIntrStatus(MCAN0_INST, gInterruptLine0Status,
DL_MCAN_INTR_SRC_MCAN_LINE_0);
printf("\nCAN_IRQ_Line0");
gServiceInt0 = true;
break;
case DL_MCAN_IIDX_LINE1: // RX FIFO 0 New Message - interrupt
/* Check MCAN interrupts fired during TX/RX of CAN package */
gInterruptLine1Status |= DL_MCAN_getIntrStatus(MCAN0_INST);
DL_MCAN_clearIntrStatus(MCAN0_INST, gInterruptLine1Status,
DL_MCAN_INTR_SRC_MCAN_LINE_1);
printf("\nCAN_IRQ_Line1");
gServiceInt1 = true;
break;
case DL_MCAN_IIDX_SINGLE_ERROR_CORRECTION:
__BKPT(0);
break;
case DL_MCAN_IIDX_DOUBLE_ERROR_DETECTION:
__BKPT(0);
break;
default:
__BKPT(0);
break;
}
}
Can anyone please help me?
If you need any more information, please let me know ;)
Thanks a lot in advance!
Matze