This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0L2228: programming issue using J-Link as programmer/debugger

Part Number: LP-MSPM0L2228
Other Parts Discussed in Thread: MSPM0L2228

Tool/software:

Hello,

I'm trying to move my project from CCS to our internal development environment, based on Segger's J-Link and related tools, like Ozone and J-Flash.

I removed all the jumpers from J14, except GND and 3V3, then connected my J-Link directly to NRST, SWDIO, SWDCLK of j14, 3V3 of J1 and GND of J2.

If I try to program the microcontroller using Ozone, I get the following message

Ozone console:

3:52:37.416 339 Debug.Start();
3:52:37.467 172 Device "MSPM0L2228" selected.
3:52:37.470 422 InitTarget() start
3:52:37.472 934 DAP initialized successfully.
3:52:37.473 004 Setting up LPM debug bits
3:52:37.475 226 InitTarget() end - Took 3.05ms
3:52:37.475 284 Found SW-DP with ID 0x6BA02477
3:52:37.478 092 DPIDR: 0x6BA02477
3:52:37.478 116 CoreSight SoC-400 or earlier
3:52:37.478 123 Scanning AP map to find all available APs
3:52:37.478 133 AP[5]: Stopped AP scan as end of AP map has been reached
3:52:37.478 140 AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
3:52:37.478 147 AP[1]: MEM-AP (IDR: 0x002E0001, ADDR: 0x01000000)
3:52:37.480 685 AP[2]: JTAG-AP (IDR: 0x002E0000, ADDR: 0x02000000)
3:52:37.480 700 AP[3]: MEM-AP (IDR: 0x002E0003, ADDR: 0x03000000)
3:52:37.480 705 AP[4]: MEM-AP (IDR: 0x002E0002, ADDR: 0x04000000)
3:52:37.480 715 Iterating through AP map to find AHB-AP to use
3:52:37.488 659 AP[0]: Core found
3:52:37.488 697 AP[0]: AHB-AP ROM base: 0xF0000000
3:52:37.488 709 CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
3:52:37.488 719 Found Cortex-M0 r0p1, Little endian.
3:52:37.488 728 FPUnit: 4 code (BP) slots and 0 literal slots
3:52:37.488 737 CoreSight components:
3:52:37.488 746 ROMTbl[0] @ F0000000
3:52:37.488 756 [0][0]: E00FF000 CID B105100D PID 000BB4C0 ROM Table
3:52:37.488 769 ROMTbl[1] @ E00FF000
3:52:37.488 781 [1][0]: E000E000 CID B105E00D PID 000BB008 SCS
3:52:37.498 378 [1][1]: E0001000 CID B105E00D PID 000BB00A DWT
3:52:37.498 401 [1][2]: E0002000 CID B105E00D PID 000BB00B FPB
3:52:37.498 407 [0][2]: 40402000 CID B105900D PID 001BB932 MTB-M0+
3:52:37.498 917 Connected to target device.
3:52:37.498 931 J-Link/J-Trace serial number: 602002504
3:52:37.531 026 ResetTarget() start
3:52:37.531 056 DAP initialized successfully.
3:52:37.531 065 ResetTarget() end - Took 5.58ms
3:52:37.531 069 Device specific reset executed.
3:52:37.531 207 Elf.GetBaseAddr(); // returns 0x0
3:52:37.532 132 Target.ReadU32 (0x00000000); // returns 0x4, data is 0x20208000
3:52:37.532 305 Target.SetReg ("SP", 0x20208000);
3:52:37.532 414 Elf.GetEntryPointPC(); // returns 0x3F58
3:52:37.532 564 Target.SetReg ("PC", 0x3F58);
3:52:39.590 818 Timeout while preparing target, RAMCode did not respond in time!
3:52:39.590 818 Failed to perform RAMCode-sided Prepare()
3:52:39.590 895 Download failed: J-Link reports an unspecified download error

If I try to program with J-Flash I get the following log:

Opening data file [myFile.hex] ...
 - Data file opened successfully (23631 bytes, 4 ranges, CRC of data = 0x1FDCD7BF, CRC of file = 0x0F5E1964)
Programming and verifying target (23631 bytes, 4 ranges) ...
 - Connecting ...
  - Connecting via USB to probe/ programmer device 0
  - Probe/ Programmer firmware: J-Link V12 compiled Dec  4 2024 17:53:50
  - Probe/ Programmer S/N: 602002504
  - Device "MSPM0L2228" selected.
  - Target interface speed: 4000 kHz (Fixed)
  - VTarget = 3.322V
  - InitTarget() start
  - DAP initialized successfully.
  - Setting up LPM debug bits
  - InitTarget() end - Took 3.00ms
  - Found SW-DP with ID 0x6BA02477
  - DPIDR: 0x6BA02477
  - CoreSight SoC-400 or earlier
  - Scanning AP map to find all available APs
  - AP[5]: Stopped AP scan as end of AP map has been reached
  - AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
  - AP[1]: MEM-AP (IDR: 0x002E0001, ADDR: 0x01000000)
  - AP[2]: JTAG-AP (IDR: 0x002E0000, ADDR: 0x02000000)
  - AP[3]: MEM-AP (IDR: 0x002E0003, ADDR: 0x03000000)
  - AP[4]: MEM-AP (IDR: 0x002E0002, ADDR: 0x04000000)
  - Iterating through AP map to find AHB-AP to use
  - AP[0]: Core found
  - AP[0]: AHB-AP ROM base: 0xF0000000
  - CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
  - Found Cortex-M0 r0p1, Little endian.
  - FPUnit: 4 code (BP) slots and 0 literal slots
  - CoreSight components:
  - ROMTbl[0] @ F0000000
  - [0][0]: E00FF000 CID B105100D PID 000BB4C0 ROM Table
  - ROMTbl[1] @ E00FF000
  - [1][0]: E000E000 CID B105E00D PID 000BB008 SCS
  - [1][1]: E0001000 CID B105E00D PID 000BB00A DWT
  - [1][2]: E0002000 CID B105E00D PID 000BB00B FPB
  - [0][2]: 40402000 CID B105900D PID 001BB932 MTB-M0+
  - Executing init sequence ...
   - Executing Reset (0, 0 ms)
    - ResetTarget() start
    - DAP initialized successfully.
    - ResetTarget() end - Took 4.62ms
    - Device specific reset executed.
   - Initialized successfully
  - Target interface speed: 4000 kHz (Fixed)
  - Found 1 JTAG device. Core ID: 0x6BA02477 (None)
  - Connected successfully
 - Checking if selected data fits into selected flash sectors.
  - ERROR: Selected Data (0x20200000 - 0x202005D0) does not fit into selected flash sectors.
More information on this can be found on the SEGGER Wiki:
wiki.segger.com/UM08003_JFlash
Disconnecting ...
 - OnDisconnectTarget() start
 - OnDisconnectTarget() end - Took 816us
 - Disconnected

Environment:

  • WIn 10
  • Ozone 3.38c
  • J-Flash 8.12a
  • Ti ARM CLANG 3.2.2

Linker file:

/*****************************************************************************

Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/

Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions
are met:

Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.

Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in the
documentation and/or other materials provided with the
distribution.

Neither the name of Texas Instruments Incorporated nor the names of
its contributors may be used to endorse or promote products derived
from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
"AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
(INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

*****************************************************************************/
-uinterruptVectors
--stack_size=256


MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00040000
SRAM (RWX) : origin = 0x20200000, length = 0x00008000
BCR_CONFIG (R) : origin = 0x41C00000, length = 0x000000FF
BSL_CONFIG (R) : origin = 0x41C00100, length = 0x00000080
}

SECTIONS
{
.intvecs: > 0x00000000
.text : palign(8) {} > FLASH
.const : palign(8) {} > FLASH
.cinit : palign(8) {} > FLASH
.pinit : palign(8) {} > FLASH
.rodata : palign(8) {} > FLASH
.ARM.exidx : palign(8) {} > FLASH
.init_array : palign(8) {} > FLASH
.binit : palign(8) {} > FLASH
.TI.ramfunc : load = FLASH, palign(8), run=SRAM, table(BINIT)

.vtable : > SRAM
.args : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)

.BCRConfig : {} > BCR_CONFIG
.BSLConfig : {} > BSL_CONFIG
}