Part Number: MSPM0C1104
Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
Hi team,
Customer use i2ctest to query MCU (they configure MCU to an i2c target with it's address 0x48) but found there is no response from MCU and they used scope to check the i2c's waveform and found SCL will become low after few clock cycles as attachment. This issue is always happened


Customer use SDK: mspm0_sdk_2_03_00_07
Questions:
Customer use M0C1104 WSON. They worry about the I2C clock and the NRST use the same pin. The I2C clock is pulled by peer device (not M0C104). Sometimes, the peer device might lost power suddenly. They worry when I2C clock is low suddenly. This will trigger NRST to M0C1104.
They also have below two questions. Please help clarify. Thank you.
- For the download firmware to MSPM0C1104SDSGR by SWD, do we need NRST pin, or we only need VDD, VSS, SWCLK and SWDIO?
- For the I2C and NREST share same pin at MSPM0C1104SDSGR, when will trigger the reset function? Will it trigger reset during I2C transmission.