Part Number: TMDSEMU110-U
Tool/software:
I am using the TI XDS110 Debug Probe connected to Code Composer Studio 12.5.0 via a USB port. When I try to Connect Target I get the following error message.
MAIN_Cortex_R5_0_0: GEL Output: ERROR: This is an HSFS device. Script must be run from R5 or A53, or boot script must be executed.
I updated the Bootloader and the firmware to 3.0.0.26, but I still get the error.