Part Number: TM4C1294NCPDT
Tool/software:
I am trying to configure the lwip 1.4.1. I using the enet_static-ip_lwip_tcpecho server example.
changes i made is I asserted the macros
#define NO SYS 1
#define LWIP_STATS 1
#define TCP_STATS (LWIP_TCP)
#define SYS_STATS 1
#define TCPIP_THREAD_STACKSIZE 1024
I included stats.h in the sysarch.h
the above modification were done in order to eliminate some compilation error.
But one error is pending is sys_mutex_t is undefined in sys.h
What to do?