Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: TCA6424
Tool/software:
Hello Team,
we are working on MCAL version MCAL_AM263Px_09.02.00 for AM263Px
we are facing difficulty in establishing communication over MCAN4 on the EVB board
we referred the example provided as part of SDK mcu_plus_sdk_am263px_09_02_00_56
Eg : :mcu_plus_sdk_am263px_09_02_00_56\examples\drivers\mcan\mcan_external_read_write
Here the IO MUX handler is handled separately and this is not part of MCAL and also when we try to refer the IO MUX handling files, there is dependency on Semaphores and other TI environment.
As we already have OS integrated and we do not need semaphore and other dependencies, Can you please provide us the IO MUX handling for MCAN4 without any additional dependency
The mcan_external_read_write example is working on CCS and communication is Up in CCS, but our application will be executed on lauterbach trace32, so we need exact IO MUX handling for MCAN4 so that we can integrate in our application.
Thanking You,
Regards,
Pradeep R