Tool/software:
Hi,
I have flashed program_application_and_wifi_fw.cfg file to the Flash memory using the Command prompt while device is in UART boot mode. I got the expected output of flashing. I have attached the image of the output.
Then, changed the boot mode to QSPI, then powered on and monitored the output in serial monitor. I'm getting 'some test has failed'. I have attached my setup and output image below. What could be the issue, the issue is in hardware or Software? Kindly give some guidance?
I tried to flash only_wifi_fw.cfg file. I'm getting the same output.