Part Number: TMDX570LC43HDK
Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
Tool/software:
Hi,
I'm tinkering with TMDX570LC43HDK(TMS570LC4357 mcu). I'm currently trying to send data via SCI using DMA but reading doesn't always work.
Here's my minimal reproducible example code:
/**
srcs unsigned char *[2] [0x0000D218 {72 'H'},0x08000294 {72 'H'}] 0x08000284
[0] unsigned char * 0x0000D218 "Hello, wor..." 0x08000284
[1] unsigned char * 0x08000294 "Hello, wor..." 0x08000288
*/
void func(void)
{
// Enable MPU first
_enable_interrupt_();
_mpuInit_();
_mpuEnable_();
// Initialize peripherals
sciInit();
dmaDisable();
dmaEnable();
uint8_t *src1 = "Hello, world!\r\n";
uint8_t src2[] = {'H', 'e', 'l', 'l', 'o', ',', ' ', 'w', 'o', 'r', 'l', 'd', '!', '\r', '\n'};
uint32_t count = sizeof(src2) / sizeof(src2[0]);
uint8_t *srcs[] = {src1, src2};
for (uint8_t i = 0; i < 2; i++)
{
g_dmaCTRL g_dmaCTRLPKT = {
.SADD = (uint32_t)srcs[i],
.DADD = ((uint32_t)&sciREG1->TD) + 3, // TMS570LC4357 is big endian
.CHCTRL = 0,
.FRCNT = count,
.ELCNT = 1,
.ELDOFFSET = 0,
.ELSOFFSET = 0,
.FRDOFFSET = 0,
.FRSOFFSET = 0,
.PORTASGN = PORTA_READ_PORTB_WRITE,
.RDSIZE = ACCESS_8_BIT,
.WRSIZE = ACCESS_8_BIT,
.TTYPE = FRAME_TRANSFER,
.ADDMODERD = ADDR_INC1,
.ADDMODEWR = ADDR_FIXED,
.AUTOINIT = AUTOINIT_OFF,
};
dmaReqAssign(DMA_CH0, DMA_REQ29);
dmaReqAssign(DMA_CH29, DMA_REQ0);
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT);
dmaSetChEnable(DMA_CH0, DMA_HW);
sciREG1->SETINT = (1 << 8) | (1 << 16);
while ((dmaREG->BTCFLAG & (1 << DMA_CH0)) == 0)
{
}
dmaREG->BTCFLAG = (1 << DMA_CH0);
sciREG1->CLEARINT = (1 << 8) | (1 << 16);
}
while (1)
{
}
}
This code does simple thing: read from src1 and send via sci, then read from src2 and send via sci again then stop.
src1 and src2 contain same data of "Hello, world!" and both are sent using dma, but only src1 transmission succeeds. For src2, remote device receives data filled with 0 instead of original data.
I suspect that the problem is related to their memory location. src1, which points to constant char array, is 0x0000D218 while src2, local uint8_t array, is 0x08000294.
But I'm not sure what exactly is causing the problem and how to solve it. I set no dma memory protection.
Thank you!