Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Team,
Making a related question. Please check the original thread for some context.
My customer is making a system project. They want to configure IPC for an empty project and have a few questions:
- Is DPL CFG in SysConfig necessary for IPC? It seems like this is necessary because when they try to load the program without it, IPC is not successful.
- In a system project, when they try to configure DPL CFG in SysConfig, it shows "Add DPL CFG (Maximum exceeded)". Please check the image below.
This seems to be related to a bug in MCU+SDK v.10.0 and older, but has been resolved in v.10.01(? not 100% sure) Please read the related thread for the bug.
- Is the reason why they cannot add DPL CFG related to the bug?
- How can they add DPL CFG to a system project manually if this is not possible via GUI?
Best regards,
Mari Tsunoda