This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: ROV tool for CPU load and memory analysis

Part Number: LP-AM243

Tool/software:

Hi there;

I would like to use ROV tool for CPU-load and memory usage analysis on my FreeRTOS project. But when I try to open ROV, I do not see "OS Kernel" section on the left menu. And I have an error message while trying to generate CPU graph.



Before running ROV, I halted the core on here;



And I use MCU+ SDK that is from the inside of Motor Control SDK. (/home/xxx/ti/motor_control_sdk_am243x_09_02_00_09/mcu_plus_sdk/)

Also this is the picture of my syscfg_c.rov.xs file




Can you please help to about running ROV tool for CPU load and memory analysis??

Best
Kadir