Part Number: MSPM0C1104
Tool/software:
According to the example of 'adc12_single_conversion', I add ADC settings (PA27) into my project.
But I can't receive any ADC12_0_INST_IRQHandler event, so I can't get any data from thermal sensor.
int main(void) {
/* Get calibrated ADC offset - workaround for ADC_ERR_06 */
gADCOffset = DL_ADC12_getADCOffsetCalibration(ADC12_0_ADCMEM_0_REF_VOLTAGE_V);
NVIC_EnableIRQ(ADC12_0_INST_INT_IRQN);
gCheckADC = false;
...
}
void ADC12_0_INST_IRQHandler(void) {
switch (DL_ADC12_getPendingInterrupt(ADC12_0_INST)) {
case DL_ADC12_IIDX_MEM0_RESULT_LOADED:
gCheckADC = true;
break;
default:
break;
}
}
I try to change the syscfg, but still not working, Could you help me to resolve this problem? Thank you.
(I can't upload my .syscfg, so I paste the content here.)
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "MSPM0C110X" --part "Default" --package "WQFN-20(RUK)" --product "mspm0_sdk@2.02.00.05"
* @v2CliArgs --device "MSPM0C1104" --package "WQFN-20(RUK)" --product "mspm0_sdk@2.02.00.05"
* @versions {"tool":"1.22.0+3893"}
*/
/**
* Import the modules used in this configuration.
*/
const ADC12 = scripting.addModule("/ti/driverlib/ADC12", {}, false);
const ADC121 = ADC12.addInstance();
const Board = scripting.addModule("/ti/driverlib/Board");
const GPIO = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1 = GPIO.addInstance();
const GPIO2 = GPIO.addInstance();
const I2C = scripting.addModule("/ti/driverlib/I2C", {}, false);
const I2C1 = I2C.addInstance();
const PWM = scripting.addModule("/ti/driverlib/PWM", {}, false);
const PWM1 = PWM.addInstance();
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");
const VREF = scripting.addModule("/ti/driverlib/VREF");
/**
* Write custom configuration values to the imported modules.
*/
ADC121.$name = "ADC12_0";
ADC121.sampClkSrc = "DL_ADC12_CLOCK_ULPCLK";
ADC121.sampClkDiv = "DL_ADC12_CLOCK_DIVIDE_8";
ADC121.adcPin0Config.$name = "ti_driverlib_gpio_GPIOPinGeneric4";
Board.peripheral.$assign = "DEBUGSS";
Board.peripheral.swclkPin.$assign = "PA20";
Board.peripheral.swdioPin.$assign = "PA19";
GPIO1.$name = "GPIO_LEDS";
GPIO1.associatedPins.create(2);
GPIO1.associatedPins[0].$name = "USER_LED_1";
GPIO1.associatedPins[0].initialValue = "SET";
GPIO1.associatedPins[0].assignedPin = "22";
GPIO1.associatedPins[1].assignedPort = "PORTA";
GPIO1.associatedPins[1].$name = "USER_ERROR";
GPIO1.associatedPins[1].assignedPin = "17";
GPIO1.associatedPins[1].pin.$assign = "PA17";
GPIO2.$name = "I2C_IRQ";
GPIO2.associatedPins[0].$name = "PIN_0";
GPIO2.associatedPins[0].direction = "INPUT";
GPIO2.associatedPins[0].interruptEn = true;
GPIO2.associatedPins[0].polarity = "FALL";
GPIO2.associatedPins[0].pin.$assign = "PA16";
I2C1.$name = "I2C";
I2C1.basicEnableController = true;
I2C1.advControllerTXFIFOTRIG = "BYTES_1";
I2C1.advAnalogGlitchFilter = "DISABLED";
I2C1.intController = ["NACK","RXFIFO_TRIGGER","RX_DONE","TX_DONE"];
I2C1.peripheral.$assign = "I2C0";
I2C1.peripheral.sdaPin.$assign = "PA0";
I2C1.peripheral.sclPin.$assign = "PA11";
I2C1.sdaPinConfig.hideOutputInversion = scripting.forceWrite(false);
I2C1.sdaPinConfig.onlyInternalResistor = scripting.forceWrite(false);
I2C1.sdaPinConfig.passedPeripheralType = scripting.forceWrite("Digital");
I2C1.sdaPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric0";
I2C1.sclPinConfig.hideOutputInversion = scripting.forceWrite(false);
I2C1.sclPinConfig.onlyInternalResistor = scripting.forceWrite(false);
I2C1.sclPinConfig.passedPeripheralType = scripting.forceWrite("Digital");
I2C1.sclPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric1";
PWM1.$name = "PWM_0";
PWM1.clockPrescale = 256;
PWM1.peripheral.$assign = "TIMG14";
PWM1.peripheral.ccp0Pin.$assign = "PA23";
PWM1.peripheral.ccp1Pin.$assign = "PA24";
PWM1.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC0";
PWM1.PWM_CHANNEL_1.$name = "ti_driverlib_pwm_PWMTimerCC1";
PWM1.ccp0PinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric2";
PWM1.ccp1PinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric3";
SYSCTL.clockTreeEn = true;
VREF.profile = "INT_1_4_V";
const ProjectConfig = scripting.addModule("/ti/project_config/ProjectConfig", {}, false);
ProjectConfig.migrationCondition = true;
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
ADC121.peripheral.$suggestSolution = "ADC0";
ADC121.peripheral.adcPin0.$suggestSolution = "PA27";
GPIO1.associatedPins[0].pin.$suggestSolution = "PA22";