This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1306: Selection suggestions for (MCU)

Part Number: MSPM0L1306
Other Parts Discussed in Thread: MSPM0L1106,

Tool/software:

Hi ti team,

Please recommend a microcontroller (MCU) that meets the following requirements:

1 ,Core:Arm 32 Bit Cortex M0+CPU,Frequency up to 24MHZ

2,64Kbytes of Flash memory,RAM≥4K

3,Two I2C-bus interfaces

4,20 PCS GPIO

5,Packages Smaller than 5*5mm

  • Hi Switch,

    According to your requirements, you need 20 GPIO+ 4 IIC IO = 24 IO PIN. Then I recommend QFN32 package which is 5mm*5mm.

    For the current device family,The MSPM0L1306 is best choice, and it is RTM already. MSPM0L1106 will be more cost-effective, while it only contains 1 IIC interface.

    Meanwhile, we do have more family device in this year, which also include several good device for your application. Please contact the TI local sales team for the detail information (Some might require NDA assigned with TI)

    B.R.

    Sal