Part Number: MSPM0G3507
Other Parts Discussed in Thread: CCSTUDIO, SYSCONFIG,
Tool/software:
In CCS Theia when I ctrl-click on function it goes to wrong source when workspace has two folders (or is it projects?)
So if I am in
project A -> main.c and I click on "init" function it takes me to the init function in the project B folder. Really hard to work when I think I am editing project A's version and later find out I was editing project B's version.
Also seems like clangd makes all editing really slow. Often keystrokes are ignore and then after a long 5-20 second delay suddenly all keystrokes are acted on. Very annoying. If I close and restart it seems to be better for a while. So I close an restart at least once a day. does clangd have a memory leak? or ? In general seems like clangd is very buggy? am I running the right version??
Details
Version: 1.4.1.1
Default VS Code API: 1.85.1
VS Code Compatibility
List of extensions
- @ccs/ccstudio 1.4.0
- @ccs/ccstudio-debug 1.4.0
- @ccs/ccstudio-getting-started 1.4.0
- @ccs/ccstudio-guicomposer 1.4.0
- @ccs/ccstudio-plugin 1.4.0
- @ccs/ccstudio-project 1.4.0
- @ccs/ccstudio-trace-config 1.4.0
- @ccs/ccstudio-trace-viewer 1.4.0
- @ccs/ccstudio-updater 1.4.0
- @theia/bulk-edit 1.46.0
- @theia/callhierarchy 1.46.0
- @theia/console 1.46.0
- @theia/core 1.46.0
- @theia/debug 1.46.0
- @theia/editor 1.46.0
- @theia/editor-preview 1.46.0
- @theia/electron 1.46.0
- @theia/external-terminal 1.46.0
- @theia/file-search 1.46.0
- @theia/filesystem 1.46.0
- @theia/git 1.46.0
- @theia/keymaps 1.46.0
- @theia/markers 1.46.0
- @theia/messages 1.46.0
- @theia/metrics 1.46.0
- @theia/mini-browser 1.46.0
- @theia/monaco 1.46.0
- @theia/navigator 1.46.0
- @theia/notebook 1.46.0
- @theia/outline-view 1.46.0
- @theia/output 1.46.0
- @theia/plugin-dev 1.46.0
- @theia/plugin-ext 1.46.0
- @theia/plugin-ext-headless 1.46.0
- @theia/plugin-ext-vscode 1.46.0
- @theia/preferences 1.46.0
- @theia/preview 1.46.0
- @theia/process 1.46.0
- @theia/property-view 1.46.0
- @theia/remote 1.46.0
- @theia/scm 1.46.0
- @theia/scm-extra 1.46.0
- @theia/search-in-workspace 1.46.0
- @theia/secondary-window 1.46.0
- @theia/task 1.46.0
- @theia/terminal 1.46.0
- @theia/test 1.46.0
- @theia/timeline 1.46.0
- @theia/toolbar 1.46.0
- @theia/typehierarchy 1.46.0
- @theia/userstorage 1.46.0
- @theia/variable-resolver 1.46.0
- @theia/vsx-registry 1.46.0
- @theia/workspace 1.46.0











icon.