Part Number: AM263P4
Tool/software:
Hi,
I understand that the ADC_CAL pins (0 and 1) are connected as channel 6 and channel 7 for every internal ADC Mux. My assumption is that, in theory, you should connect 2 known constant voltages to these pins to then be able to calibrate out differences between the internal ADC muxes. This is evident by the table included below taken from the technical reference.

My questions are:
Can they be used as regular single-ended analog inputs?
Can I connect a variable signal to the ADC_CAL0 pin and just read it on every adc mux?
Is the raw ADC count measurement for the ADC_CAL pins available to be fetched from the ADC peripheral?
Is there any auto-calibration that occurs on the ADC front end to try to automatically calibrate out the difference in the ADC_CAL measurement between cores that could be affected by a changing signal on the ADC_CAL pin?