Part Number: MSPM0G1506
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi
Could you provide information on the baud rate error percentage for the UART communication module in the MSPM0G1506 when using the internal clock source? We are considering avoiding the use of external LFCLK and HFCLK due to cost constraints. Specifically, we need to know if using the internal LFXTAL (32KHz) is sufficient, or if the external LFXTAL is mandatory. Additionally, as this UART interface operates in PD0 (low power domain), what would be the maximum input clock frequency for the UART peripheral, and are there any limitations in achieving higher baud rates such as 115200 or greater?
With Regards
Ilan