Part Number: MSPM0G1505
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi - we are using the ADC12_0 in Sequence mode in a MSPM0G1505. We have set up ADC12 with the following parameters:
1. Clock Source - ULPCLK
2. Sample Clock divider Div by 8
3. Conversion Mode: Sequence
(a) Set Conversion Start Address - 0; End Address - 7
(b) Enable Repeat Mode is checked
(c) Sampling Mode is Auto
(d) Trigger Source is Software
5. ADC Conversion Memory 0-7 Conversion are set to use Sampling Timer 0 as Sample Period Source.
6. Enable Interrupts is set to MEM0 Result loaded Interrupt
In terms of reading the ADC .. this is the Pseudo Code:
process ADC registers