Other Parts Discussed in Thread: TMS570LS20216
Hi, i was looking at Hercules MCUs but i could not find any great difference between RM4 family and TMS570. The later is qualified for automotive applications.. but i belive that is not enough difference to create two distinct families. There are also differente peripherals, but thats not enought either as thet got differencie within the families. Any comment about that? I will probably go for TMS570 due to the automotive rating, but i want to make sure the real difference.
Also an extra question. I was looking at TMS570 USB stick and i noticed that there is a pad for placing a connector for the J-tag. Is that for real? Can i debug an external device with the kit? If yes, is there any special requirement as specific jumper setting to accomplish this task?
Thank you!