Part Number: LP-MSPM0G3507
Tool/software:
Hello.
I want to send say a 1k block of data to a master...the 3507 is a slave.
The master is SPI clocking at 16 MHz.
I can't see how I can do this as a "single" block....since the FIFO is just 8 bytes there will be a "gap" if I either reload the FIFO in software or even DMA.
Effectively I want to DMA to SPi FIFO but never overwrite...
Regards
Phil