Part Number: TMS570LC4357
Tool/software:
In main.c I initialize one pin of the DMM as an output and set it as follows:
#define dmmREG ( ( dmmBASE_t * ) 0xFFFFF700U )
uint32 pinMask = 0;
dmmREG->GLBCTRL = 0x5; // ON/OFF = 0101 in GLBCTRL
pinMask |= ( 1U << 12 );
dmmREG->PC0 &= ~pinMask; // Set to GIO
dmmREG->PC1 |= ( 1U << 12 ); // Set direction
dmmREG->PC4 = ( 1U << 12 ); // Set pin 12 High atomically
and it works!!
My problem is that when I try to set the same pin via a periodic FreeRTOS task I get a memory access protection fault:
dataEntry
b dataEntry
Can I get some help please?