This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, Team.
I would like to know the clock sequence when powering on.
After powering on, the clock is input (XI if a crystal is used), and then the PoZ reset is released. Are there any timing specifications?
Also, if a crystal is used, is it correct to understand that XO is output from the microcontroller after the reset is released?
Jpanese memo
パワーオン時のクロックのシーケンスを教えてほしい
電源オン後にクロック入力(水晶を使用する場合、XI)、さらにその後PoZリセットが解除になると考えられるが、タイミング規定はあるのか
また水晶を使用している場合、XOはリセット解除後にマイコンから出力される認識でいいか
Hello Yohei-san,
After powering on, the clock is input (XI if a crystal is used), and then the PoZ reset is released. Are there any timing specifications?
No there is not, but if the oscillator is not able to start correctly then the device will typically fail to boot. It may be possible to get the device boot in limp mode but it wouldn't really be able to run a high performing system like that.
Also, if a crystal is used, is it correct to understand that XO is output from the microcontroller after the reset is released?
I am not sure I am fully understanding this question, but if you mean will the MCU I/O for XTAL_XO be functional and work with an active oscillator, then yes it would. It will begin functioning after reset is released and as soon as the crystal starts to input into the MCU.
Best Regards,
Ralph Jacobi