Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: N2HET BR instruction not set HETFLG bit

Part Number: RM57L843

Tool/software:

Hi,

I wrote a HET code where I branch using BR instruction when Carry flag is set (generated by add/sub during wraparound) with IRQ turned on. However, I noticed that the HETFLG bit is not being set when the condition is satisfied. When I run it on the simulation, I see that the HETFLG is set correctly but not when I execute it on the actual hardware. Ant pointers on what I could be missing?

Thanks,

Ravi