This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Occasionally fails to detect that the mibspi's RXEMPTY flag == 0.

Part Number: TMS570LC4357


Tool/software:

When using mibspi in master mode, not utilizing interrupts. After configuring and initiating the RX RAM transfer, I use  while (rx_ram.RXEMPTY (flag bit 31) != 0) to detect whether the reception is complete.While this approach works effectively in most cases, there are occasional instances where the RXEMPTY == 0 state persistently fails to be detected. 

I have noted the entry MIBSPI#139 in the errata manual: "Mibspi RX RAM RXEMPTY bit does not get cleared after reading." However, the issue I am encountering appears to be related to the RXEMPTY flag not being set to 1 promptly. Additionally, no other transfer groups have been configured in my setup.