Part Number: MSPM0G1107
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Dear support team,
I have downloaded several times our custom specific secondary_bsl_uart Project based on ti project.
We use our own custom Board.
We didn't change any Project specific settings nor params regarding NVM Parameter. When trying to debug the project we get permanently the
Error connecting to the target: (Error -6305)
message. Methods like Start Project-less Debug leads just to not ending functions when calling FactoryResetPasswordAuthentication_Auto
Test Connection with MSPM0G1107.ccxml delivers following screen.
What was suspicous in this whole process, is that after unsuccessfull download Device Passwords showed all 0x0 which wasn't the same as configured in project.
Memory reading is impossible all adresses just delivers ????????
Factory Reset Mode Policy and Mass Erase Mode Policy is both enabled in project.
Any Ideas, could it be an migration problem of our project as we exchanged the CCS version several times over the last year and actually we use Version 20.0.2.5__1.6.2
Some other project settings like parameters for hex file generation were for example lost after migration.

After upgrade the 8 was an empty field.