Part Number: AM263P4
Other Parts Discussed in Thread: AM6442, TMDSCNCD263P
Tool/software:
Hi Team,
I would appreciate your clarification on a few questions regarding the AM263P4 device.
We are planning to establish a SPI connection (not using the boot mode SPI) between the AM6442 and AM263P4 devices. Is it possible to update the image over this SPI connection, which is separate from the OSPI.
Additionally, we have RGMII connections between both devices. In your opinion, which interface—RGMII or SPI—would be more efficient for the update process, or which one is more complicated to manage?
The AM263P4 datasheet states that it has 6 UART ports with RS485 support, but I noticed an additional UART available from the Industrial Domain. Is it possible to use this UART for console purposes during the debugging process?
Can i add PSRAM and Flash Devices on OSPI Interface in AM263P4 Device for Memory extension ? If Yes, could you please provide examples if available ?
Thanks
Dilip Kumar