Part Number: TMS570LS3134
Tool/software:
Hi Champs,
Is the SPI self-test function of the TMS570LS3134 supported by all SPI? Or is it only supported by MIBSPI? Thanks!
BR
Julia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3134
Tool/software:
Hi Champs,
Is the SPI self-test function of the TMS570LS3134 supported by all SPI? Or is it only supported by MIBSPI? Thanks!
BR
Julia
Hi Julia,
Memory related self-test functions are only available for MibSPI because MibSPI have RAM buffer to store multiple SPI packets whereas this RAM buffer not available in normal SPI, so these memory related self-tests are only available for MibSPI.

There are some other diagnostics like loopback are available for SPI as well, you can find the definitions of these functions are available in SDL:
SAFETI_DIAG_LIB Driver or library | TI.com

--
Thanks & regards,
Jagadish.