Part Number: MSPM0L1304
Tool/software:
Hi,
In the MSPM0L1304 datasheet, there is a contradiction in the pin functions of package RTR, between Figure 6-8 and table 6-1:
Pin 8: The table says it supports ROSC function, while the figure shows only PA2 (unlike other package drawings),
Pin 2: The figure does not state it supports VREF+ (unlike other package drawings),
Pin 11: The figure shows it supports PA14 but the table doesnt.
I may have missed other contradictions.
I understand some of the pins, like NRST and PA1 are dual bonded, but that is not what I'm asking.
What are the correct capabilities of each of the pins of the RTR package?
Thank you.