Part Number: TMS570LS2124
Tool/software:
Hi Champs,
Now customer is using DMA interrupt, they configured two DMA interrupt , both of which are BTC type (Block transfer complete). There are 16 DMA channels (from 0~15), but according to the description in Table 16-47 of TRM, BTCA only uses 0~5 bits to represent 0~15 channels, instead of 16 bits to represent them one by one.

So if both channel 1 and channel 4 are configured as BTC interrupts, when channel 1 and channel 4 trigger the DMA interrupt at the same time, will BTCA read the wrong channel number and cause the wrong interrupt? Or will this causing interrupt missing?
Customer's meaning is, although BTCA is read then clearly, if it is interrupted at the same time, channel 1 BTCA will be set to 0b010, and channel 4 BTCA will be set to 0b101, so if it is interrupted at the same time, will BTCA be set to 111, that is, it will become the interruption of channel 6?
Now customer find that the program work well when only one DMA interrupt is configured. When two DMA interrupts are configured, one of them will occasionally fail to trigger. They want to know why this issue is occurring.
Thanks!
Best Regards,
Julia