Part Number: AM263P4
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I have 4 PWMs (0-3) that are to be perfectly aligned. PWM0 generates syncout at zero and all other pwms (1-3) have phase enabled and syncin is configured to EPWM0 syncout. I have also set all TBPHS to 0.
When looking with a scope, PWM0 and PWM1-3 are out of sync by approx 5ns (or 1 clock cycle @ 200MHz). So it looks like by the time SYNCOUT is generated from PWM0 and received by the other PWM SYNCINs, 1 clock cycle has passed.
Pic shows PWM0 compared to PWM2. PWM2 is lagging PWM0.

Is there a recommended solution to get the downstream PWMs synced up exactly to PWM0?
Here is a dump of the registers:

Thanks for the support