This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: GPIO power on abnormality

Part Number: AM2432

Tool/software:

Hi ALL:

   1、 Recently, we found during testing that the GPIO Y7 of AM2432 defaults to external pull-up, with the system initialization configured as input. After the system initialization is complete, the voltage level drops below 3.3V, the 10K pull-up level drops to 2.3V, and the 4.7K pull-up level drops to 2.7V; Why did the 1K level drop to 3.18V when pulled up?

    

   Figure 1 we board ID circuit,GPIO Y7 pull up by 10k

    

   Figure 2 we test scope GPIO Y7 pull up by 10k

  

  Figure 3 we test scope GPIO Y7 pull up by 1k

2、There is a hook during the power on process of the MCU-RERNT and RESET-REQz pins

  Figure 4 MCU_RESENT POWER ON

 Figure 4 RESENT_REQz POWER ON

 Figure 4 RESENT_REQz  and 3.3V POWER ON

3、GPIO has a recoil when powered off。