Part Number: LP-MSPM0G3519
Tool/software:
Hello team,
we are using MCAL : MCAL_MSPM0_00.02.04.00 package
SDK : mspm0_sdk_2_04_00_06 version
we are working LP-MSPM0G3519 board, we need to execute tests on trace 32, so when we checked the CPU LP-MSPM0G3519 is still not supported by trace32 software.
Can you please share us the cmm scripts that can be used to run the initialize the LP-MSPM0G3519 Ti launch pad board and also please lets us know if any additional jumper settings that we need to take care when we are connecting external JTAG debugger from lauterbach
As per the board, we see there are two XDS-110 IN(J103) and XDS-110 OUT ports(J102), please let us know where we need to connect the external JTAG debugger and also jumper J101 handling
Thanking you.
Regards,
Pradeep R