Part Number: TMS570LC4357-SEP
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
Hello,
I want to use 4 RS-485 in full duplex mode with RE and DE control. Is it possible with this MCU? Can I use LIN1 and LIN2 for RS-485?
Also, can I configure analog inputs as digital input or output? Out of the 41 availabe ADC channels, I am planning to use 28 as analog inputs, and remaining as Digital Input/Output.
I also want to understand pin config. in the below attached photo. Does it mean that I can use ePWM1A on D9 while also using GIOA[5] as an I/O on B5?

Lastly, if I am using only 4 pins (SCK, MISO, MOSI, CS) on SPI1, can I use the remaining pins as normal GPIO? Also, why are there 2 pairs of SOMI and SIMO?