Part Number: AM2434
Tool/software:
Hi,
we are working on FreeRTOS, when adding a PCIe driver, program will crash in Pcie_open().
Platform: AM243xEVM as RC
SDK Version: ind_comms_sdk_am243x_09_00_00_03
Question 1: Is the configuration of Outbound address correct? What do Base Address and Target Address refer to respectively?
Question 2: Due to Pcie_open() is in SDK and cannot be debugged into. Is there any method to investigate the reason of program crash?
Question 3: MPU ARMv7 configuration as right picture, is there any correlation between the configuration of MPU REGION and PCIe?