Part Number: MSPM0G1107
Other Parts Discussed in Thread: ADS114S08B,
Tool/software:
Hello,
I'm considering handling GPI (interrupt) via a pin shared with the MISO on the SPI bus. Actual use case is to read "Data Ready" signal from the ADC (ADS114S08B) via a bus shared with MISO.
Regarding MSPM0G1107/1507, are there any options to implement that? Is it the feasible way that changing the peripheral function at runtime, every sampling? Or (possibly), can read logic signals under SPI peripheral configuration with special backup resister or something like that?
Thanks.