Part Number: TMS570LC4357
Tool/software:
Hello,
What is the maximum baud rate that can be achieved with the TMS570LC4357? Additionally, if I set VCLK to its maximum value of 110 MHz, what baud rate and error rate can I achieve? Are there any other factors that should be considered before increasing VCLK?
Also, can I disable the Lockstep mode and use both cores parallely to increase the processing capability?
Thanks in advance.
Regards,
Dhir