Part Number: AM2632
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Support Team,
I am encountering an issue with the I2C communication between the AM2632 and a humidity/temperature sensor(NSHT30-Q1DNR). I would appreciate your guidance to resolve this problem.
Problem:
-
Write works, but read fails: After sending the slave address (with R/W=1), the sensor ACKs, but SCL stays LOW.
-
I have tried various read and write operations, and each read operation has the same response, so I cannot output clk completely
- I am certain that slave is functioning normally
-

Setup:
-
Sensor: at 7-bit address 0x44.
-
I2C speed: 400 kHz (standard mode).

-
Pull-ups: 4.7kΩ on SDA/SCL.

Question:
Why would SCL stay low after a slave ACK during a read? Could this be a master configuration issue or sensor behavior?
Attachments:
-
Logic analyzer capture (
SCL_stuck.png).
Thanks for your help!
Best regards,
zx