This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100 and IAR Compiler

Hi all,

I am using RM48 with XDS100 in the IAR Compiler and I can't see the variable values in the Watch window. I change the values but this values in the window don't change, is 0 always.

Somebody know that is happening?

tks,

 

Alessandro

  • Hi Alessandro,

    Just tested. There is no problem to show the variable value in watch windows. I am using IAR workbench 6.21.1 (free version). 

    1. Can you erase the flash correctly using XDS100 under IAR IDE? Just to make sure your tool configuration is correct.

    2. If yes, can you program the RM48x sample blinky project to the flash and see the blinky LED (after programming and reset)?

    3. After you change the variable value, please re-compile project, re-load the code to memory to check the new value.

    Regards,

    QJ

  • Hi QJ,

    I see that all values into registrations is changed, only variable values didn't change in the watch window.

    I saw my XDS100 configuration and when I clear the "user flash loader(s)" box and chose the "attach the program", the changed values can be see, but I can't save the new software version in memory.

    What's the right configuration in the Debugger tab? Or have other configuration to see?

    tks,

     

    Alessandro

  • Hi Alessandro,

    I have the same problem with the variable values. Can you please report this bug to IAR? I will submit a ticket to IAR too. Thanks

     

    Regards,

    QJ 

  • QJ,

    I reported this problem. They told me this problem is interface XDS100 working with IAR. That this problem don't happen with the JTAG interface (the problem is our kit haven't this connector....).

    Anyway, now I compile and save my program by "User flash loader(s)" and after change this configuration to "Attach ro program".

    While don't solve this problem, lets this way.

    If I have news, I will post here.

     

    Alessandro

  • Dear all,

    the above described issue of IAR debugger with XDS100 interface has been fixed in the release/version: 6.40.2 (IAR EWARM)

    I am not sure whether this version can be already downloaded from IAR website. I was forwarded by IAR support to some FTP server - thanks for that!

    Temporary directory (reachable till 2012-08-03) ftp://files.iar.com/pub3/4afeae33066e545da2440dc6242fcb98

     

    Cheers,

    Jiri