Tool/software:
I have one question regarding the TMS570LS1224 FMEDA Excel document.
Are the ISO 26262-5:2018 Requirements 9.4.1.2 and 9.4.1.3 considered in evaluating the MCUs FMEDA?
Especially, i'm interested in whether a single failure modes residual fault rate violates the 0,1 FIT barrier ("one-tenth of the value corresponding to failure rate class 2").
This is unfortunately not obvious from the FMEDA Excel document.