This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: use Port0 with ICSS and the other port as CPSW?

Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG, AM2432

Tool/software:

Hi,

Is it possible to use one port on the Launchpad board as ICSS and the other port as CPSW?

We would like to run the EtherCat example: “extercat_slave_cia401_demo_am243x_lp_r5fss0-0_freertos” on one CPU with one port,

and the example “enet_cpsw_typServer…” on the other CPU with the other port.

I think the problem is in the Sysconfig either only TI Industrial Comms or only TI Networking can be configured, depending on which SDK is selected!

                    

Not together. How can I do that?

Regards,

Alexander