This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: How to use AD1IN[6] on J10 Pin 48 instead of the light sensor?

Part Number: TMS570LS1224


Tool/software:

Hello,

I need to use the AD1IN[6] input on my Hercules  LaunchPad. However, I noticed that the onboard light sensor is tied to AD1IN[6], and I want to use an external input through J10, header pin 48 for my application.

I applied 0V to J10, pin 48, but the ADC reading still reflects the light sensor's value.

Is there a way to disable the light sensor so that I can correctly read my external input on J10, pin 48?
Any help would be appreciated!

Thx

Ariel