Other Parts Discussed in Thread: MSP430F5529, INSTASPIN-BLDC, DRV8301, DRV8312, LM3S818, TMS320F28035, CONTROLSUITE, DRV8302
Hello,
I'm in the initial phase of a new project and I would like your suggestion to select the correct micro.
The application is ebike type motor driver and the main requirements are:
1/ BLDC sensored (3 hall effect) and sensorless operation
2/ input control monitoring (4 buttons, 1 encoder signal, 1 PWM input)
3/ USB and bluetooth communication
4/ field upgradable sw
5/ low cost
low power is also impprtant as this is battery operated, however the battery is quite large so we can compromise a little on this requirement....
Thanks,
Andrea