This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: CSS 20.1.0: How to create a new project for ICSSG1-PRU1 or change an example from ICSSG0-PRU0 to ICSSG1-PRU1

Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I am experimenting with the mcu_plus_sdk_am243x_10_01_00_32\examples\pru_io\adc\ads85x8 demo which runs one of the projects on ICSSG0-PRU0.  I want to create a project to run on ICSSG1-PRU1 as it has pins available that I want to control as well. I cannot find an example that is assigned to ICSSG1-PRU1 and can't figure out how to change any of the demo projects from the SDK to ICSSG1-PRU1 since it is locked in the project properties editor.

I have tried changing the target in .syscfg by using "SWITCH" device, but my CCS studio locks up after clicking OK in the Migrate dialog box.