Part Number: AM2432
Tool/software:
Hi
Customer want to implement voltage detect 5V via this USB0_VBUS pin. Is it feasible?

Regards
Zekun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Zekun,
Thank you for the query.
The VBUS is used as part of the USB interface.
VBUS is connected through a divider as per the data sheet for the device.
For host, this is optional.
Regards,
Sreenivasa
Hello Zekun,
Thank you.
Are you able to share the use case for me to check. As i understand, the VBUS IO does not monitor the VBUS when configured as host.
A USB power switch with OC indication is recommended to be used. This pin can be connected to any of the SOC IO to detect USB VBUS fault.
Regards,
Sreenivasa