Part Number: AM2612
Tool/software:
Hi TI Support Team,
I want to use the CLKOUT of AM2612 to provide clock(e.g.:50Mhz) for external devices, but I couldn't find a configurable option in syscfg. How should I proceed

Best regard
zx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ZX,
Please expect a delay in response since the expert is Out-of-office.
Regards,
Shaunak
Hi zx

You can refer to the above section from TRM, on how to program CLKOUT.
Regards,
Akshit
ZX,
I have used this code to enable clock out on the LP:
#define MSS_TOP_RCM_U_BASE (0x53200000U)
#define MSS_TOP_RCM_LOCK0_KICK0 (0x00001008U)
#define MSS_TOP_RCM_LOCK0_KICK1 (0x0000100CU)
#define MSS_TOP_RCM_CLKOUT0_CLK_SRC_SEL (0x00000C00U)
#define MSS_TOP_RCM_CLKOUT1_CLK_SRC_SEL (0x00000C04U)
#define MSS_TOP_RCM_CLKOUT0_DIV_VAL (0x00000C08U)
#define MSS_TOP_RCM_CLKOUT1_DIV_VAL (0x00000C0CU)
#define MSS_TOP_RCM_CLKOUT0_CLK_GATE (0x00000C10U)
#define MSS_TOP_RCM_CLKOUT1_CLK_GATE (0x00000C14U)
#define MSS_TOP_RCM_CLKOUT0_CLK_STATUS (0x00000C18U)
#define MSS_TOP_RCM_CLKOUT1_CLK_STATUS (0x00000C1CU)
#define IOMUX_U_BASE (0x53100000U)
#define IOMUX_IO_CFG_KICK0 (0x000002A4U)
#define IOMUX_IO_CFG_KICK1 (0x000002A8U)
SOC_controlModuleUnlockMMR( SOC_DOMAIN_ID_MAIN, 5 );
SOC_controlModuleUnlockMMR( SOC_DOMAIN_ID_MAIN, 6 );
*(volatile uint32_t*)(IOMUX_U_BASE + IOMUX_IO_CFG_KICK0) = 0x83E70B13;
*(volatile uint32_t*)(IOMUX_U_BASE + IOMUX_IO_CFG_KICK1) = 0x95A4F1E0;
*(volatile uint32_t*)(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_LOCK0_KICK0) = 0x01234567;
*(volatile uint32_t*)(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_LOCK0_KICK1) = 0xFEDCBA8;
*(volatile uint32_t*)(0x531001E8) &= 0xffffff00U; // 0x10u (enable CLKOUT0)
*(volatile uint32_t*)(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_CLKOUT1_CLK_SRC_SEL) = 0x444; // Select the clock source
*(volatile uint32_t*)(MSS_TOP_RCM_U_BASE + MSS_TOP_RCM_CLKOUT1_DIV_VAL) = 0x999; // Divide by 10
This should work for you.
-Jason