Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I am trying to get the application image verification by bootloader/DMSC to run.
A few prerequisites:
- Using MCU+ SDK for AM243x 9.2.0.50
- Using SysConfig 1.20.0
- Using custom flash W25Q64JV.
- Using AM2432BSFFHIALXR Sitara on custom hardware.
The issue is:
- If I set the setting "Disable Auth For Application Image" then it works as intended.
- But if I uncheck this setting then Bootloader_verifyMulticoreImage() inside Bootloader_parseMultiCoreAppImage() fails.
- However, I assume that the application image is properly signed by makefile_ccs_bootimage_gen.
I have attached a minima example of 3 projects (bootloader, system image and application image). You can check my flash settings there. I have also attached my devconfig.mak.
I also tried already a few things like switching "app_degenerateKey.pem" for "rom_degenerateKey.pem" or "custMpk_am64x_am243x.pem" and vice versa etc. and switching GP for HS without success.
I would appreciate it if somebody could look over my projects. I tried to keep them as close as possible to the original example projects.
Thank you.
Kind regards,
Martin