Part Number: AM2434
Tool/software:
Hello,
we are currently working with the AM2434 board, which has a single assigned MAC address from TI stored internally on the chip. We intend to utilize the ethernetip_adapter_generic_device_rgmii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang project for an Ethernet/IP daisy chain configuration.
I have a couple of questions regarding the MAC address configuration:
Is it necessary to assign a separate MAC address for each port on the AM2434 when implementing the Ethernet/IP daisy chain?
The adapter demo project appears to be using the MAC address stored in EEPROM. How can I modify the project to utilize the MAC address directly from the chip instead? Where is on chip MAC address located?
Any guidance on these points would be greatly appreciated.
Thank you for your assistance!
BR,
Matej Liska.