Part Number: AM2432
Tool/software:
Hi Team,
we are working on AM2432 Sitara Custom board (Slave Device) with DP83822 PHY for Ether CAT protocol.
We used two ethernet ports in our board.
We are able to assign IP address for both MAC and able to ping it. Post that we loaded the slave device with Ether CAT code and checked with Ether CAT master Twin CAT (Individual ports) it works perfectly.
For the Ether CAT Daisy chain connection, we take the two custom boards and made the below connection
Our custom boards PHY address for port 1 address is: 3 and Port 2 address is: 1, we configured port 2 as Input.
1'st Board ---- Port 2 (Input) to PC
1'st Board ---- Port 1 (output) to 2nd Board (Port 2) Input port.
After made this connection, scanned the device in Twin CAT master only one box only detected. We attempt multiple combination of connection as well.
Is that any specific configuration required for daisy chain of Ether CAT Am2432 slave devices.?
Regards,
Chockalingam