Part Number: MSPM0G1506
Other Parts Discussed in Thread: SYSCONFIG,
Tool/software:
Hello.
I have a question about the BOR settings.
I have set the BOR threshold level to 1 for the MSPM0G1506 in Sysconfig.
When I checked the BOR setting of the MCU while it was running, the threshold level was 1.
However, the MCU is resetting when the power supply voltage is between 1.59V and 1.62V.
After investigating, I think that BOR threshold level 0 might be applied.
Why isn't BOR threshold level 1 being applied?
Thanks.